REC.TRIGSLOPE
Description
REC.TRIGSLOPE sets the recorder trigger slope. This parameter is not used when REC.TRIGTYPE is 0 or 1.
| Value | Description |
|---|---|
| 0 | Negative |
| 1 | Positive |
Examples
Code
Trigger the capture on a positive rate of change.
-->REC.TRIGSLOPE 1
Context
For more information see Scope.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
1 |
|
Data Type |
Integer |
|
See Also |
REC.TRIG, REC.NUMPOINTS |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
|
Copyright © 2018 Kollmorgen |
|